6/3/2021 10:18 AM | |
Joined: 6/19/2018 Last visit: 5/6/2024 Posts: 10 Rating: (0) |
I need some guidance on how to use the the IE/PB link as a PN/DP coupler. Looking through the forum I came across this post, saying it is possible: Couplers DP & PN - Entries - Forum - Industry Support - Siemens The manual linked in the above post mentions using the RDREC instruction to read the I&M data record, but not much else. The setup I have is a 1515T connected to the IE/PB Link on the ethernet side, and a 314C-2DP on the profibus side. I have the IE/PB link setup as network gateway in standard mode (I believe this is the correct setting), and i want to exchange 64 bytes of data between the two systems, but I don't understand how to configure the exchange. Do I have to use Put/Get Functions? Or do I need to use RDREC/WRREC or RD_REC/WR_REC? |
6/4/2021 7:14 AM | |
Joined: 6/19/2018 Last visit: 5/6/2024 Posts: 10 Rating: (0) |
Here are the screenshots. Other than the settings shown I'm not sure what needs to be changed. Right now I just don't understand how to address the IO data.
AttachmentScreenshots.zip (670 Downloads) |
6/4/2021 10:36 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (819) |
pls be kind show more cfg screenshots. Where is your mentioned 64 Byte data exchange defined? Your screenshot is cutted so no other infos visible. Hope then we can give you better help... Update: here is list of some examples with IE/PB link: List examples IE/PB link |
Last edited by: Duris_I at: 06/04/2021 11:56:27With best regards... |
|
Follow us on