6/6/2021 5:09 AM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
Hi everyone, I faced an issue " Insert (1739:460) "symbolname" operand not permitted" when copying chart from PLC A user project to PLC B user project. Solution: When copy and paste chart with channel driver block and symbol connection connected, ensure the symbol name and its address is defined properly in target PLC. For example, PLC A - PT001 is defined as IW 10 , WORD. but in PLC B, PT001 might define as PT001, I0.0, BOOL. When copy the chart from PLC A to PLC B, operand not permitted might happen to block you from copy over the chart. Refer to the attached picture for the pop out. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to2 thankful Users |
Follow us on