6/10/2021 6:57 PM | |
Joined: 4/4/2019 Last visit: 1/28/2024 Posts: 1 Rating: (0) |
Hello, How can we connect the SENTRON PAC3200 ModBus TCP with Desigo CC V5 ? With best regards, |
6/11/2021 8:46 AM | |
Posts: 39 Rating: (8) |
Hi, you have to create Modbus TCP driver first. Next step is Modbus TCP network. Use default Modbus TCP integration template which can be found in C:GSMprojects (or something like that) Here is the following link for more help. Integrating Modbus TCP Power Devices into the Management Platform (desigoccecosystem.com) CSV File for Modbus Device Import (desigoccecosystem.com)
|
Last edited by: AutoGen_9341646 at: 06/11/2021 08:50:58 |
|
Follow us on