6/11/2021 1:53 PM | |
Joined: 11/22/2017 Last visit: 4/4/2024 Posts: 2 Rating: (0) |
I developed an C# based (Windows Form) application to exchange Digital I/O with Instance CPU (Type 1500), Connection established successfully. Also I can able to trigger Input address (starting from Byte '1'), But I cant able to trigger input address in Byte '0' (i.e. from I0.0 to I0.7, not able to trigger from application) Any syntax need to write to trigger the address in Byte '0' ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/14/2021 09:35:34New subject after splitting |
|
6/14/2021 11:17 AM | |
Joined: 11/22/2017 Last visit: 4/4/2024 Posts: 2 Rating: (0) |
Hello Duris, Firstly Thanks for you quick reply... My requirement is I created a Windows form (with push buttons etc..) and try to establish communication with PLCSIM advanced v2.0 (which is already done) to test the PLC Program Even I triggered the inputs from Application, its working fine except the Addresses (I0.0 to I0.7), I surprised why address in IB0 not able to trigger, rest all inputs can able to trigger & working fine Herewith I added the Program codes, Communication Snapshot for your reference AttachmentSnapshot.zip (125 Downloads) |
Follow us on