6/14/2021 3:38 PM | |
Joined: 12/16/2016 Last visit: 12/29/2021 Posts: 32 Rating: (1) |
Hello guys, good morning! i would like to join the conversation!!! i have a machine with 3 module FM 372-2, and i want to know some things! first: i cant see the program of 357-2 module when i upload program from s7-313C cpu, why? second: in each module have a blue card with code: 6es7 951-1km00-0aa0, its a memory card! can i exchange one for another in each module? or can i exchange one module for another? i ask it because the machine is with problem in the axis and i cant monitorate it! thank you !! best regards! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/15/2021 10:20:18New subject after splitting |
|
6/15/2021 10:21 AM | |
Joined: 8/21/2014 Last visit: 4/19/2024 Posts: 949 Rating: (13) |
Closed, cause question posted twice. The second thread with the subject [FM357-2] is published within the conference [SIMATIC S7-300 / S7-300F]. Best regards The Helping Hand
|
My Forum is the place to personalize your profile, |
|
Follow us on