6/21/2021 3:16 PM | |
Joined: 6/4/2010 Last visit: 4/18/2024 Posts: 370 Rating: (125)
|
Dear Ivadyz, It looks like there are other users with the same issue. There is an FAQ describing this issue. Please see: https://support.industry.siemens.com/cs/ww/en/view/109797040 A final solution is planned for V5.0 QU1 (and V5.1). QU01 should be released in the coming month(s). There may be workaround for the “run time error” message showed from time to time. You may try the workaround below and report in the forum, if the workaround solves the issue. Other users may be interested in your feedback. Workaround: Open the default.ldl configuration file (for system manager and summary bar configuration) and set the “SnapInInactivityTimeoutInMinutes” to “0” (zero) to disable the inactivity check. See the attached screen shot for further information. Best regards, Albis |
8/3/2022 5:27 PM | |
Joined: 5/4/2022 Last visit: 11/16/2023 Posts: 1 Rating: (0) |
Albis, Screen shot should be attached. |
Follow us on