6/18/2021 6:42 AM | |
Joined: 5/5/2020 Last visit: 6/30/2023 Posts: 40 Rating: (0) |
Dear Experts, I tried to add ET200SP to Simotion D425-2 DP/PN project , i made hardware configuration and selected the value of ET200SP exactly which i have (as shown in NetPro attached picture) but after downloading the project and simotion turned to run , the ET200SP gives flash red light (as shown in attached video) and when i go to online i see the ET200SP is run but there is an error (as shown in Online attached picture ) . Kindly could any one explain to me how to solve the problem ? and is there any project example for simotion with io device ? . Regards AttachmentET200SP.zip (270 Downloads) |
6/21/2021 10:49 PM | |
Joined: 9/27/2006 Last visit: 4/18/2024 Posts: 12256 Rating: (2664) |
Hello eory; For digital I/O modules on the ET 200SP, there are 4 BaseUnits you can use,depending on whether you intend to start a new potential grou or not, and whether you need auxiliary connections for your I/O. The screenshot below illustrates this. It is taken from the ET 200SP manual: https://support.industry.siemens.com/cs/ww/en/view/58649293/145129311371 I find ths presentation a good introduction the ET 200SP Base Uinit selection and installation, maybe it can clarify some issues: https://realpars.com/et-200sp-base-unit/ Hope this helps, |
Last edited by: dchartier at: 06/21/2021 22:50:11 |
|
Follow us on