6/27/2021 1:30 PM | |
Joined: 3/14/2008 Last visit: 9/17/2024 Posts: 2095 Rating: (936)
|
Hi, This is the sign that show the logic runtime sequence of blocks. If the sign appears between two blocks, this means that the first block (where the output is connected) is installed in the runtime group later than the block to where the input is connected. The system shows this sign and you can solve it by changing the block order or to use: Optimize run sequence so all blocks are corrected in terms of runtime. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to5 thankful Users |
Follow us on