7/1/2021 10:52 AM | |
Joined: 8/20/2018 Last visit: 9/30/2022 Posts: 1 Rating: (0) |
Dear all, I am currently doing Modbus setup at standalone S7-400 PCS7 V8.0 SP2 to read Modbus reading from MOX RTU MX606. I am facing the problem which I wanna do programming to read from this MOX RTU using RCV_341 block but I can't find it in PCS7 AP Library V80. I tried to install PCS7 AP Library V71 as RCV_341 and SND_341 only have in this library. Installation was done by using V8.0 Installation CD in the additional product. As below, now RCV_341 exist. I have update the block types. I try to include this block in my CFC but there was an error occur when doing the compilation. Tried this also Any suggestion/solution to overcome this issue? If cant view all photos, can refer to my pdf in attachment. Attachmentrcv341.pdf (27 Downloads) |
Last edited by: EryFx at: 07/01/2021 10:53:35Last edited by: EryFx at: 07/01/2021 10:55:27 |
|
Follow us on