7/5/2021 4:34 PM | |
Joined: 5/20/2021 Last visit: 4/8/2022 Posts: 55 Rating: (0) |
Hi, i use a pump to suck water from the tank and pump it back into the network .my goal is to keep set point at 25 psi .my question is how to configure the parametre of my PI to let the speed of my pump stable because its going from 250 till 1000. thanks. Attachmentprincipale.zip (293 Downloads) |
7/5/2021 4:50 PM | |
Joined: 12/18/2014 Last visit: 9/25/2024 Posts: 33835 Rating: (4205)
|
I don't understand why you make always a new topic for the same project. control speed peristaltic pum flex pro serie A2VYou have a adjustable pump. You want to a constant pressure by using a PI controller. A PI controller can't give a constant value at his output. The output value depents on the value of the pressure sensor. |
7/6/2021 7:55 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject control speed peristaltic pum flex pro serie A2V is published within the conference LOGO! - Projects. Jen_Moderator |
Follow us on