7/6/2021 11:12 AM | |
Joined: 6/16/2016 Last visit: 2/29/2024 Posts: 15 Rating: (0) |
Hi, I send the PM Thank you |
7/6/2021 2:19 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, since I couldn't detect the node which throws the uncaught exception I simply goolged for it. It came out that zlib is a submodule of core nodeJS and that this is known from version 6 to 14 (see here). The linkes issue is still open, so I guess there is no solution. What's also mentioned in this issue it that zlib is called when using websocket communication (this comment). Is it possible that there is communication from a server while a client is not available for example? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on