7/15/2021 5:58 PM | |
Joined: 9/11/2013 Last visit: 2/29/2024 Posts: 13 Rating: (0) |
Dear experts, I have one machine with the next configuration: PLC - 315 PN/DP - ES7315-2EH14-0AB0 3x DIGITAL INPUT 1x Digital input 4x - Sinamics DCM DC converter (6RA8013-6DV62-0AA0) Comunication Profinet with a Sclance switch (6GK5108-0BA00-2AA3) 1x HMI 6AV6647-0AD11-3AX0 Our problem: When we power on the machine the PLC try to start but it stays in stop and "SF". If we change from run to stop and then to run the PLC start with no error. PLC diagnostic: Event 5 of 108: Event ID 16# 49A0STOP caused by parameter assignment error or unpermissible difference between preset and actual configuration: startup disabledNo relevance for user (SDB no.): 1000No relevance for user (Z2): 07fe (Z3): 0004Previous operating mode: STARTUP (warm restart)Requested operating mode: STOP (internal)External error, Incoming event04:21:56.470 PM 07/13/2021(Coding: 16# 49A0 FF64 C17B 03E8 07FE 0004) Event 6 of 108: Event ID 16# 4301Mode transition from STOP to STARTUPSTOP due to: Power failureStartup information:- Time for time stamp at the last backed up power on- Single processor operationCurrent/last startup type:- Automatic warm restart after backed up power onPermissibility of certain startup types:- Manual warm restart permitted- Automatic warm restart permittedLast valid operation or setting of the automatic startup type at power on:- Automatic warm restart after backed up power onPrevious operating mode: STOP (internal)Requested operating mode: STARTUP (warm restart)Incoming event04:21:56.400 PM 07/13/2021(Coding: 16# 4301 FF46 C772 494E 0810 7710) I saw that the sinamics only pass to online after this Event so i thing that the problem is in the comunication with the PLC and the converter's. My question is how I can prevent this error and startup the PLC when the power goes up. I send the all diagnostic in attacment. Thanks and best regards. AttachmentPLC Diagnostic.pdf (361 Downloads) |
Follow us on