7/21/2021 9:26 AM | |
Joined: 3/3/2020 Last visit: 1/26/2024 Posts: 10 Rating: (1) |
Hi all, I have been following the simple example outlined in this video https://youtu.be/A0L_5_sIH5U and the example in "500 Process Automation (PA) – University Learn-/Training Documents V9.0" chapter P01-04 Individual drive functions. Whatever I have tried I cannot seem to drive an Input (I0.0) on the the PLCSIM. I'm pretty sure that SIMIT is aware that PLCSIM is there and running because if I start the SIMIT simulation without PLCSIM in RUN mode then it shows me the error that PLCSIM is not running. But when I run it I still cannot drive any of the signals. The versions and my problem is shown in the attached image. Has anyone got any ideas on what else to check? |
Last edited by: mookie1983 at: 07/22/2021 02:28:07 |
|
8/5/2021 12:40 PM | |
Joined: 11/15/2018 Last visit: 12/12/2023 Posts: 7 Rating: (4) |
Hello, can this FAQ be the solution for your problem? Why can the communication between SIMIT and PLCSIM not be established? |
This contribution was helpful to1 thankful Users |
Follow us on