7/19/2021 9:21 AM | |
Joined: 3/14/2008 Last visit: 3/28/2024 Posts: 2059 Rating: (924)
|
Hi, PCS7 uses Simatic Manager and is bound to a specific version. It basically the same but with some additions but that depends on the installed applications like AS-OS engineering, Simatic BATCH, RC and CFC/SFC. You can still use "normal" editors like STL, FB, SCL . SCL is commonly used for creating your own blocks. When PCS7 is installed, the projects are created as PCS7 projects, meaning some things change like downloading DB individually is not allowed. But you can also create STEP7 projects in PCS7 environment. |
Last edited by: Oreca at: 07/19/2021 09:23:59If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
7/19/2021 1:22 PM | |
Joined: 5/3/2018 Last visit: 12/5/2023 Posts: 56 Rating: (0) |
Thanks Oreca, is LAD also possible in Step 7 PCS7 version? Thanks |
7/19/2021 1:29 PM | |
Joined: 3/14/2008 Last visit: 3/28/2024 Posts: 2059 Rating: (924)
|
Hi, Yes, also LAD, I did not put it in my previous post, not meaning it was excluded. Sorry. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on