7/21/2021 9:11 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello Mauricio; Your screenshot indicates that it is the load memory (MCC) of your CPU thst is full, which means your MCC has reached its capacity limit. The work memory (internal RAM, whee the program code is executed) is still at 50% capacity. For a description of the different types of memory areas in your S7-300, please open section 4 of the following document: https://support.industry.siemens.com/cs/us/en/view/7302326 The work memory of the S7-300 is fixed, determined by the technical specifications of the CPU, and cannot be extended. https://support.industry.siemens.com/cs/ww/en/view/19102565 Hope this helps, |
Last edited by: dchartier at: 07/21/2021 22:39:33Last edited by: dchartier at: 08/03/2021 12:00:22 |
|
This contribution was helpful to2 thankful Users |
Follow us on