4/1/2010 2:44 PM | |
Posts: 7 Rating: (0) |
I am having some trouble with the horn configuration. we have multiple operators, each with multiple stations. I have setup the horn configuration to allow horn acknowledgement from any station (you ack the horn, it silences the horn on other machines). Is there a way to have the Acknowledge Alarm button also acknowledge the horn? Also, I am seeing something weird.... When an alarm comes in and, for example, I silence the horn (but do NOT ack the alarm). When I ack the alarm, the horn starts playing again! I have to re-ack (or silence) the horn to make it stop. Any ideas? We are running PCS7 v7.1 (APACS OS v7.0), with redundant servers, a CAS server, and 12 clients. Attached are screenshots of the CLIENT application configuration. The Server application does NOT have any Horn configuration..... thanks in advance for any help!!
Attachmenthornconfig.zip (661 Downloads) |
5/7/2012 8:33 AM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello Umair, How is the horn editor configured for single-user stations, servers, redundant servers and client OS stations in SIMATIC PCS 7 / WinCC? |
Ammy |
|
7/24/2021 5:09 AM | |
Posts: 1 Rating: (0) |
|
Follow us on