2/20/2017 1:27 PM | |
Joined: 5/6/2010 Last visit: 5/12/2024 Posts: 1965 Rating: (273) |
Hello, the highest numbers are DB - 255 Please look at the link, there are the technical data of the PLC. https://support.industry.siemens.com/cs/pd/285014?pdti=td&lc=en-WW I hope this helps. regards |
This contribution was helpful to1 thankful Users |
2/20/2017 2:28 PM | |
Joined: 11/17/2010 Last visit: 4/2/2024 Posts: 216 Rating: (39) |
Hi, I'm not sure about data given by CaOd (Sorry CaOd). It seems those values represent the number of blocs allowed and not the number range assigned to the FC or FB. Unfortunately, I'm not able to find this range for CPU 6ES7315-1AF03-0AB0. .Example for CPU 6ES7315-2AG10 : Number of FC allowed = 1024 but number range is 0 to 2047 (FC0 to FC2047) Number of FC allowed = 1024 but number range is 0 to 2047 (FB0 to FB2047) Look at this link to compare : |
Follow us on