8/2/2021 3:19 PM | |
Joined: 4/28/2015 Last visit: 4/30/2024 Posts: 3345 Rating: (377)
|
Hi, which kind of PLC are you using? The IOT2040 can read data from your PLC either via S7 or OPC UA (being an OPC UA client) and store the data in a database. There is two application examples showing exactly this use-case (one for node-red, one for C++). What data do you want to display? Current values or historical ones from the databas? Both should be possible with the node-red dashboard. The IOT2050 does have NodeJS, C/C++ and python onboard. With those environments you can use every functionality being available as Open Source. Best regards! |
Last edited by: bergmanu at: 08/02/2021 15:20:57Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on