7/19/2021 9:30 AM | |
Joined: 3/14/2008 Last visit: 4/18/2024 Posts: 2064 Rating: (926)
|
Hi, The PH is sometimes tricky. You can set different levels for the block icons in the Plant View of the OS project. If you right click a hierarchy folder->Plant Hierarchy->Create/Update block icons, you can set the number of lower hierarchy folders under: "Lower hierarchy levels included". If you set this to 0, the block icons are only created for the picture that is present in the folder where the block resides. If you set this to 1, the block icons are created for the picture and includes all block icons from one sublevel below. You can however create plant hierarchy folders without any picture in it, the system thus does not create block icons then. This way, you can "play" a little to get the correct plant hierarchy you want.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
Follow us on