8/9/2021 9:31 AM | |
Posts: 198 Rating: (60) |
Hello, After downloading the AS wide interconnection in Netpro, it is also important to perform a complete compile and download the Charts folder on the respective AS. Ensure that the blocks are OB34 (200ms) or lower to ensure your connection between the blocks in the two AS is valid before performing the compilation and download. If you are still facing the issue, please send appropriate screenshots to get a better resolution. Please refer section 10.8.2 "Setting up AS-wide interconnections" in the CFC Manual for further information on AS wide interconnection recommendations. CFC Manual Link Hope this helps! |
Last edited by: TechnoBlaze at: 08/09/2021 09:36:38Last edited by: Jen_Moderator at: 08/09/2021 13:01:02Optimized link. |
|
Follow us on