8/18/2021 6:33 PM | |
Joined: 2/8/2015 Last visit: 7/10/2024 Posts: 462 Rating: (9) |
Hello dear all, Can everybody explain me how Deos the cemat tool "C_MIG_V80" works? Regards Tekabi |
8/20/2021 1:37 PM | |
Posts: 198 Rating: (60) |
Hello Tekabi, In Cemat V7.1 SP1 some already existing block parameters have been changed to Structures. These are the group/route links, the actual value and the external setpoint of the damper positioner and the setpoint input and output function of C_DRV_1D. With PCS7 V8.0 these interconnections are converted into textual interconnections. Some of these interconnections should are rewired to the new structure outputs. The Excel tool C_MIG_V80.XLS does this rewiring to the new structures. Because of this, the process object view must be exported before the block update. The Excel tool C_MIG_V80.XLS change e. g. the existing interconnection to the measured value output MV to the new structure measured value output PV_Out. You may refer the below mentioned manual for more information under section 'Update of S7 program' https://support.industry.siemens.com/cs/ww/en/view/64877628 |
Last edited by: The Helping Hand at: 08/20/2021 13:57:05Optimized link. |
|
Follow us on