8/19/2021 1:09 PM | |
Joined: 7/14/2016 Last visit: 9/12/2023 Posts: 387 Rating: (27) |
Hello, I am using os single station in my project. I have used OS single station license but it is showing license error of OS server basic. Why this license is nedded? I also checked as per above document, it should not be required. Thanks in advance... Kbv. ------------------------------------------------------------------------------------------ |
Last edited by: Kbv at: 08/19/2021 13:11:24Last edited by: The Helping Hand at: 08/19/2021 15:42:52New subject after splitting Don't just think in terms of solutions... |
|
8/19/2021 6:21 PM | |
Posts: 567 Rating: (106) |
Hi Kbv. Check the project typ in the project properties (WinCC Explorer). Maybe it is not set to Single-User project. If it it is you can try to change it to Multi-User. Close the project. Open it again and change back to single user. BR Ralfinio
|
Follow us on