8/25/2021 6:09 PM | |
Joined: 9/1/2015 Last visit: 1/20/2024 Posts: 15 Rating: (0) |
Hello, I had D445 installed in the machine. several days ago, D445 was broken. we found the sub-contract to fix it. After that, there was alarm F30062 in ALM. I got the help from this forum to upgrade the FW of D445 from 4.1 to 4.3. After this upgrade, all the led was flashing during the machine running and BCD display "F". If i switch off and switch on D445. it's normal. The attachment is the DIAG log. AttachmentDevice Diagnostics(1).zip (184 Downloads) |
Last edited by: 金枪鱼 at: 08/25/2021 18:23:52 |
|
8/25/2021 6:15 PM | |
Joined: 9/1/2015 Last visit: 1/20/2024 Posts: 15 Rating: (0) |
here is the video, when the problem happened.
Attachment2bb292770f4f06c34d20cdba13c68849.zip (203 Downloads) |
8/26/2021 3:14 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
F in BCD means System Faiilure (FW crashed) here you should open a Service Request |
8/26/2021 6:35 AM | |
Joined: 9/1/2015 Last visit: 1/20/2024 Posts: 15 Rating: (0) |
Thanks for your help! this D445was 10 years old. may be it is not compatible with the new firmware 4.2 &4.3? |
8/26/2021 6:47 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2983)
|
if is not compatible then it would not boot up. the old D445 was supported up to FW V4.4 if i remember correct |
8/26/2021 7:10 AM | |
Joined: 9/1/2015 Last visit: 1/20/2024 Posts: 15 Rating: (0) |
Dear sir, can you explain this fault information. |
Follow us on