9/1/2021 5:08 AM | |
Joined: 3/27/2017 Last visit: 4/1/2024 Posts: 11 Rating: (0) |
Hello all friends. I also have a SIMOTION D425-2 kit that also fails to restart itself after about 15-30 minutes of operation. I can feel the temperature on its side with my hand. It is very hot but the cooling fan only turns on for 1-2 seconds and then turns off. And I can't find the parameters to turn on or adjust for it.. It's too bad when the heatsink temperature is too high, while we have a set of fans with excellent heat dissipation, they lie still and don't. do nothing. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/13/2021 14:03:24New subject after splitting TruongVu |
|
Follow us on