9/20/2021 1:38 AM | |
Joined: 11/26/2020 Last visit: 8/10/2022 Posts: 2 Rating: (0) |
Hello How can i make classes in hmi comfort |
9/20/2021 2:34 AM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685) |
Hello moutafashraf; Have a look at this article: - SITRAIN course: SIMATIC WinCC (TIA Portal) on the machine level for Comfort Panels and WinCC Runtime Advanced - now also available as Online Training https://support.industry.siemens.com/cs/us/en/view/109758624 Sitrain is the training division of Siemens, they offer in-person and distance classes on PLCs, HMI, SCADA software, drives, etc.. in many countries indicated here: Hope this helps |
Last edited by: dchartier at: 09/20/2021 13:15:58 |
|
9/20/2021 4:57 PM | |
Joined: 11/26/2020 Last visit: 8/10/2022 Posts: 2 Rating: (0) |
In induosoft scada i used a feature called “classes” to make one screen for controlling 10 motor so i made classes of motor and defined start,stop and coil then assigned start push button to tage Motor[number].start and stop pushbutton to Motor[number].stop and coil to Motor[number].coil so i want to do this in hmi, how?
|
9/20/2021 5:29 PM | |
Joined: 9/27/2006 Last visit: 9/23/2024 Posts: 12282 Rating: (2685) |
Hello morafashraf: Very sorry, it seems I misunderstood your original question. Please make sure you provide sufficient information with your next questions so we may provide the correct answers. As per your description of "classes" in Indusoft SCADA (I am not familiar with Indusoft), and the following technical reference it seems Indusoft uses compound tags to create instances of motor controls, for example. http://download.indusoft.com/81.2.0/IWS+v8.1%2BSP2+Technical+Reference+(LT).pdf In TIA Portal, the design of repeatable instances of motor controls (again, for example) uses hat is known as "faceplates", graphic libraries that group representations and indirect tags linked to a control object, saved to a project library. You will find definitions and examples of faceplates in the TIA Portal v16 system manual: https://support.industry.siemens.com/cs/az/en/view/109773506/109113832331 This application example should give you more infrormation on the subject: - Creating Faceplates with WinCC Runtime Advanced and Comfort Panels https://support.industry.siemens.com/cs/de/en/view/68014632 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 09/20/2021 22:17:14Last edited by: dchartier at: 09/21/2021 21:27:10 |
|
Follow us on