6/26/2016 6:29 PM | |
Joined: 3/30/2011 Last visit: 9/22/2024 Posts: 736 Rating: (256) |
Hello, interesting question...... I tried for about ten minutes without results... it seems that it is not possible........ Look also here.........jc44627 is waiting for a tia update... Then I try the same with winccflexible and KTP600...... in runtime rectangle is displayed over trend. Last hope is that some other user knows some workaround........ or we have to wait tia v14. Best Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
6/28/2016 3:56 PM | |
Joined: 1/21/2013 Last visit: 9/4/2024 Posts: 4620 Rating: (707) |
Hello javed, It seems that TP 700 have this function (if you use this) have a look: 6AV2124-0GC01-0AX0 - Product Details - Industry Mall - Siemens WW Complex image objects ● Number of complex objects per screen 20 ● f(x) trend view Yes I have not tried it yet |
7/11/2016 2:26 PM | |
Joined: 7/19/2011 Last visit: 9/20/2024 Posts: 262 Rating: (5) |
Still same issue. Anyone please give some suggestions. |
JAVED AKHTAR |
|
7/14/2016 2:26 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello javed88, it's a normal behavior in WinCC Advanced:
There is a workaround for WinCC Professional, but you can't use it in Advanced, because it uses screen windows. I don't know a workaround in WinCC Advanced. Even putting the rectangle and/or the control into a faceplate together with another control doesn't help. Pop-ups can't be turned transparent. Would it work for you if you change the axis values (dynamically), so the whole visible area is the plotting area (and with another change of the axis values you can go back to an overview view)? |
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
Follow us on