Industry Online Support
Technical Forum
9/22/2021 12:51 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
hi TNT_HPDQ, If the PLCs are in the same subnet you can also use I device communication. Have a look to this application sample: Configuration and Application of the PROFINET I-Device FunctionIf they are not in the same subnet there is the open user communication which can also be routed: How do you program the TSEND_C and TRCV_C instructions for open user communication over the integrated PROFINET interface of the S7-1200/S7-1500 CPU?hope this helps, regards, |
FCK WAR! |
|
Follow us on