9/24/2021 7:36 PM | |
Posts: 257 Rating: (77)
|
Hello SIOS Forum Community Recently, the question of how SIMATIC controllers can be connected to EtherNet/IP has been asked more frequently. The Ethernet Industrial Protocol (EtherNet/IP) is an open standard for industrial networks. EtherNet/IP is used to transmit cyclic I/O data as well as acyclic parameter data. EtherNet/IP was developed by the ODVA (Open DeviceNet Vendor Association) and standardised in the international IEC 61158 series of standards. The following SIOS contribution is wonderfully suitable here: EtherNet/IP Scanner - Connecting Ethernet/IP Peripherals to SIMATIC S7 Controllers. In this context, we would also like to give a hint about the ET 200SP MultiFieldbus interface module IM155-6MF HF with firmware V5.0.3. The ET 200SP peripheral system can be operated on a PROFINET controller as well as on an EtherNet/IP or Modbus TCP controller. The topic page "MultiFieldbus - An overview of the most important documents and links" contains further information, e.g. on EtherNet/IP. Note The procedure described in this article refers to the time of writing this article (status: July 2021). Yours sincerely SIMATIC International Technical Support Hub |
Last edited by: Jen_Moderator at: 09/27/2021 10:08:57Edited text for better reading. |
|
Follow us on