10/8/2021 8:40 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
Please refer Inverter (DC-AC) Compact Type manual. |
Last edited by: Jen_Moderator at: 10/08/2021 10:15:46Optimized link. |
|
10/8/2021 9:24 AM | |
Joined: 6/28/2016 Last visit: 4/18/2024 Posts: 22 Rating: (0) |
Thanks for your response. Reading this manual at page 322 I can find what I am searching for. But above every stage there is a sheet number, in my case sheet 318. Is this a refererence to another manual, for example vc34_kompend? |
10/8/2021 10:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872) |
I guess you are talking about right side bottom letters e.g. s81 or r1 etc etc. If so these are sheet numbers of function diagram (refer page no 300 of same manual) Like same, you can find more details of setpoint channel of control V/F type i.e. p100=2, on sheet 316, 317 & 318. Please refer SIMOVERT MASTERDRIVES, VECTOR CONTROL, COMPENDIUM manual function diagram no 316, 317 318 (i.e. manual page no 536,537,538) Hope this helps. |
10/8/2021 11:17 AM | |
Joined: 6/28/2016 Last visit: 4/18/2024 Posts: 22 Rating: (0) |
Ok it is what I was expected but I wanted to know if there is another manual because it senses to me quite strange to immediately set the additional setpoint 2 to zero, So if I give only additional setpoint 2 to the drive an OFF3 command will propably cause an overvoltage to the drive, isn't like this? |
Follow us on