10/13/2021 3:49 PM | |
Joined: 8/24/2021 Last visit: 4/19/2024 Posts: 7 Rating: (0) |
Hi everyone I'm using cpu s7 300 & cp341 as modbus rtu master. But unfortunately the communication doesn't establish and neither of CP341 LEDs blink. I have inserted the dongle and installed essential softwares (CP PtP Param v.5.1.15 and modbus master 3.1sp8) on PCS7. FB8 has status code 16#301. Diagnostic buffer of CPU & CP has no fault. I'm totally confused. I have attached some pictures of my work and would be thankful if you could take a look and help me as soon as you can. Thank you so much... AttachmentCp341 problem-1.zip (184 Downloads) |
10/15/2021 8:49 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050)
|
Hi, M.Ar, have you seen the application sample: Master-Slave Communication with Modbus RTU for S7-300 and ET 200S Systemshope this helps, regards, |
FCK WAR! |
|
This contribution was helpful to1 thankful Users |
Follow us on