10/17/2021 5:07 PM | |
Joined: 9/27/2006 Last visit: 4/24/2024 Posts: 12257 Rating: (2665) |
Hello Iyyappan; Have a look at this document, Released Modules for PCS 7 v9.0 SP1. https://support.industry.siemens.com/cs/ww/en/view/109754965/107445060363 It details the compatibility of network componnts (mostly Profibus and Profinet) with this version of PCS 7, and alo (in the S7-400 section) the art number of the CPU 410-5H (he CPU part number, not the bundl you have puchased: 6ES7 410-5HX08-0AB0 V8.2 for example). You can check the screenshot below to see that ths version of PCS 7 supports your IM 153-2, with all its functionnalities. You can find similar documents on the forum site, if you are using a different version of PCS 7 and wish to have an absolute answer to your question. Hope this helps, Daniel Chartier |
Follow us on