10/19/2021 3:30 PM | |
Joined: 8/16/2021 Last visit: 1/4/2022 Posts: 15 Rating: (0) |
Hello, Is there any possible to connect LOGO with ULCT 900/108 E Light Curtains? Can the logo handle it like an ordinary sensor? [snip] Attachment1121.pdf (393 Downloads) |
Last edited by: AlanGocolTe at: 10/19/2021 15:31:04Last edited by: The Helping Hand at: 10/20/2021 09:01:58Removed link and added file as an attachment. |
|
10/19/2021 3:57 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
The LOGO! is not approved for safety applications. |
10/22/2021 8:53 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Without safety function use this diagram. |
This contribution was helpful to1 thankful Users |
10/22/2021 9:03 AM | |
Joined: 8/16/2021 Last visit: 1/4/2022 Posts: 15 Rating: (0) |
Could you tell me which wire of these 7 is the signal wire that should be plugged into the digital input? |
10/22/2021 9:06 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Are you not a electrician? You can't read this simple diagram? |
10/22/2021 12:44 PM | |
Joined: 8/16/2021 Last visit: 1/4/2022 Posts: 15 Rating: (0) |
Thank you very much for your help, currently my task is to get to know how the sensors work and to program them. I have never asked such questions from here before. [snip] ... --------------------- |
Last edited by: CS Moderator at: 10/25/2021 08:07:27 |
|
Follow us on