10/11/2021 4:07 PM | |
Joined: 10/9/2021 Last visit: 8/21/2024 Posts: 20 Rating: (0) |
Hello All, I am very beginner with PCS7 installation. This is first time i am installing PCS7. I am now about to install PCS7 V9.1 with OS as Windows 10 LTSC version 1809 with build no. 17763.2183. I have following questions before starting with installation: 1. Will SQL server 2017 get automatically installed during Installation of PCS7 package or do i need to install it separately before installation of PCS7. 2. I have read quiet about the patch management and windows updates. Also compared my Windows update history with patch excel file. However, i am not sure if i have fulfilled this requirement or not. Regards, Shree ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/12/2021 08:22:17New subject after splitting |
|
This contribution was helpful to1 thankful Users |
10/12/2021 8:36 AM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150) |
Hello Shree2893, SQL server 2017 will get automatically installed in PCS7 V9.1 Before installation of PCS7 V9.1 please make sure that windows OS are up to date. To know more about PCS7 V9.1 installation, please go through the below link PCS 7 - PC Configuration (V9.1) Note: Before installation of PCS7, some Windows features have to be enabled in order to meet seamless installation (All are covered in attached link). |
This contribution was helpful to1 thankful Users |
12/2/2023 2:28 PM | |
Joined: 1/4/2021 Last visit: 9/20/2024 Posts: 2 Rating: (0) |
Good afternoon. Have you already solved the problem? tell me how exactly?
|
Follow us on