10/21/2021 7:47 AM | |
Joined: 5/3/2018 Last visit: 1/5/2023 Posts: 8 Rating: (0) |
Hi I would like to clarify what is defined as IO device? 1.) ET200MP/ ET200SP 2.) Simocode/third party drives with Profinet interface 3.) Another PLC onfigured for PUT/GET data exchange (S7 Comms) 4.) Modbus TCP communication 5.) Scalance switch configured in network topology Do they all count towards that "Number of connectable IO Devices, max." number ? Regards, Justin ------------------------------------------------------------------------------------------ |
Last edited by: CS Moderator at: 10/21/2021 12:53:52New subject after splitting |
|
Follow us on