10/22/2021 6:28 AM | |
Joined: 1/11/2019 Last visit: 9/17/2024 Posts: 758 Rating: (150) |
Hello Mn6453shabad, Usually in the upgradation perspective, there are two options: with or without the utilization of the functionality of the newer version (7.1 in this case). It is recommended to go through this manual perform the upgradation based on your requirement: Also have a look at the following FAQ, it includes the manuals for updating to all other versions: On that note, Siemens only provides recommendations and procedures with relevance to the PCS7 product line. PCS 7 can only run on operating systems that have been approved for PCS 7 (but Siemens does not recommend whether or not you could upgrade the OS or not - Before installing PCS7 v7.1, it is important to ensure one of the recommended OS is installed). It is recommended by PCS7 to follow the guidelines for recommended Operating systems and IPC product line for a trouble free upgrade experience. Hope this helps! |
This contribution was helpful to1 thankful Users |
Follow us on