10/25/2021 7:46 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Which device is your client? |
10/25/2021 7:50 AM | |
Joined: 6/15/2021 Last visit: 6/6/2023 Posts: 48 Rating: (0) |
A raspberry pi using Node-Red. The node is "node-red-contrib-s7" |
10/25/2021 7:53 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
Are you shure that the syntax "DB1,INT1406" is correct? I think it must be "DB1, DBW1406". |
10/25/2021 8:20 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066)
|
In the LOGO! program you must give the NAQ a address in the VM area, e.g. VW0. Then can you read it as DB1 ,WORD0. Take a look at this web site, especially the section "Notes on Logo! 8".: node-red-contrib-s7 |
This contribution was helpful to1 thankful Users |
Follow us on