10/20/2021 3:50 PM | |
Joined: 1/19/2016 Last visit: 2/8/2023 Posts: 7 Rating: (1) |
Hi all: I have a problem with the graph overview in HMI. We make some graph with it's own graph overview and simulate it with PLCSIM and HMI Simulator and I can see graph status in HMI and operate with it correctly. When I download it in real PLC and real HMI it doesn't work. It seems that it have no connection, but I can see the state of all tags of the Instance DB. I check the state of "Internal parameters..."and it's ok. Can anybody help me? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/21/2021 06:34:19New subject after splitting |
|
10/25/2021 3:46 PM | |
Joined: 2/17/2020 Last visit: 4/25/2024 Posts: 992 Rating: (169) |
Okay, thanks for checking! Do you have a ProDiag license and have you transferred it to the HMI panel? it's the only thing I can think of that justifies the behavior of the GRAPH Overview. Under what circumstances is a ProDiag license required in the WinCC (TIA) Runtime? |
A rating will be well appreciated. |
|
10/26/2021 8:26 AM | |
Joined: 1/19/2016 Last visit: 2/8/2023 Posts: 7 Rating: (1) |
Good morning Yes, we have installed Prodiag license. Thank you. |
Follow us on