10/28/2021 1:46 AM | |
Joined: 10/28/2021 Last visit: 11/12/2021 Posts: 5 Rating: (0) |
Hello, out of curiosity and the fact that I've been struggling with the download to the HMI. Were you also responsible for downloading the project to the HMI? I thought I did everything right but after I compile and try to download to the HMI I have no luck. I did have errors, apparently with internal tags? I ran the message extractor prior and when we had errors we went back through the logic and fixed them, so we thought? Any ideas on where I'm going wrong or what I'm missing? I can also give more detail if needed. Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 10/28/2021 09:06:39New subject after splitting |
|
10/28/2021 11:20 AM | |
Joined: 8/12/2020 Last visit: 4/25/2024 Posts: 41 Rating: (3) |
Hi ControlsDude25, Can you publish a screenshot of the error you mention? BR, Hugens. |
10/28/2021 4:41 PM | |
Joined: 3/2/2016 Last visit: 4/2/2024 Posts: 72 Rating: (14) |
Have you tried to delete the IM folder of the project? |
10/31/2021 4:12 PM | |
Joined: 10/28/2021 Last visit: 11/12/2021 Posts: 5 Rating: (0) |
After the logic was updated we were able to download to the HMI. This was the result, telling us to configure screen. |
Follow us on