12/3/2021 10:06 AM | |
Joined: 5/28/2018 Last visit: 3/14/2024 Posts: 29 Rating: (0) |
I don't know much about programming, but you can add two counters, one of which will record each ton, the only thing I do not know how to save the transition mass, between 990kg and 1 ton AttachmentWeight_0BA8.Standardеареааре.lsc.zip (377 Downloads) |
12/3/2021 10:09 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32880 Rating: (4064)
|
If you mean you have a solution, then make it. |
12/3/2021 12:15 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
See attachment for a correct version to add tons. All calculations are made around one arithmetic block with 3 analog multiplexers. One multiplexer adds the actual weight, the second one is for reset and the third one to subtract 1000.0kg, when the threshold trigger exceeds 999.9kg, the right values are important for correct values. Check the program for bugs i might have missed. Regards, Scorp P.S. This program is not correct, see next entry AttachmentTotalWeight1.zip (419 Downloads) |
Last edited by: Scorp at: 12/03/2021 19:34:09 |
|
12/3/2021 2:18 PM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32880 Rating: (4064)
|
The same problem as the program from Avtovazov: Is the weight exactly 20.0 kg then works it correct. But is the weight e.g. 19.7 kg .... AttachmentTest_weight.zip (367 Downloads) |
12/3/2021 7:35 PM | |
Joined: 2/22/2008 Last visit: 2/22/2024 Posts: 2698 Rating: (206) |
You are right, i have forgotten the off value of the threshold trigger, which also must be 9999, same as on value. Regards, Scorp AttachmentTotalWeight2.zip (384 Downloads) |
Follow us on