12/2/2021 3:51 PM | |
Joined: 11/1/2021 Last visit: 12/2/2021 Posts: 7 Rating: (0) |
Hi Everyone I hope you can help a newbie - I have looked and found similar threads but not been able to identify the problem. This is my first project and I cannot get the 24v DC outputs to work. Unit is an S7-1200 DC/DC/DC (214-1AG40-0XB0). I have connected +24v to .3L and have also tried with and without negative on 3M, there is no voltage coming on the output terminals. The program is working fine and you can see the lights are on indicating that the outputs should be live. Link to photos and short video. [snip] If you can give any guidance it would be appreciated. Many thanks in advance. AttachmentFiles.zip (318 Downloads) |
Last edited by: BlueDuck at: 12/02/2021 15:54:00edited to open links in new window Last edited by: BlueDuck at: 12/02/2021 19:45:41Last edited by: Jen_Moderator at: 12/03/2021 08:55:53Removed links and added files as an attachment. |
|
12/2/2021 7:49 PM | |
Joined: 11/1/2021 Last visit: 12/2/2021 Posts: 7 Rating: (0) |
I have updated the links to pictures in the first post and they should work now. |
12/2/2021 10:08 PM | |
Joined: 11/1/2021 Last visit: 12/2/2021 Posts: 7 Rating: (0) |
The only forum I have used that seems to limit 1 picture per post? |
12/2/2021 10:09 PM | |
Joined: 11/1/2021 Last visit: 12/2/2021 Posts: 7 Rating: (0) |
output wiring |
12/2/2021 10:09 PM | |
Joined: 11/1/2021 Last visit: 12/2/2021 Posts: 7 Rating: (0) |
input wiring |
Follow us on