12/7/2021 9:13 PM | |
Joined: 9/27/2006 Last visit: 9/18/2024 Posts: 12282 Rating: (2684)
|
Hello dbpathak; Inside Step 7, the basic iddea is that you need to create a new block (in the Blocks directory), determine if it is an FC, an FB, a DB or an OB,. Once that is done you give the new block a name (this is the number it will be recognised with, say FC120) and the prameter it requires. Then you compile it (it then appears in the blocks list), program it and download it to the PLC. This is the way the Step 7 and WinCC v16 manual explains it, for FCs and FBs in detail: https://support.industry.siemens.com/cs/ww/en/view/109773506/22243936907 And from the same manual, how to create a DB: https://support.industry.siemens.com/cs/ww/en/view/109773506/90269291915 Hope this helps, |
Last edited by: dchartier at: 12/07/2021 21:15:44 |
|
This contribution was helpful to1 thankful Users |
12/9/2021 3:19 PM | |
Joined: 3/30/2020 Last visit: 9/19/2024 Posts: 4767 Rating: (978) |
Hello. I think you will be able to find what you are looking for in the example program: Have a look in the forum for follow-up questions relating to the example. Use the search facility within the forum looking for "excel openness". Without knowing the details of the above sample and lacking Openness experience.. I would have created LAD/FBD/SCL code with a program in the XML format that Openness recognises. The XML file can then be imported as a code block. I do know with small scripts developed with OpennessScripter that the API exists that can export code blocks to XML and import XML as code blocks. |
Last edited by: qwazee at: 12/09/2021 15:22:35Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
Follow us on