12/2/2021 8:06 PM | |
Joined: 8/2/2019 Last visit: 1/12/2022 Posts: 12 Rating: (0) |
Hello everyone. After the movement function (MC_MOVERELATIVE) has been executed, some small reference remains, as a result of which the drive rotates slowly. Sometimes the drive starts to rotate as soon as MC_POWER is turned on. Link to video: [snip] The drive is controlled by Profinet. A TTL 1024 AB encoder (no zero mark) is connected to the inverter. CPU 1510SP-1 PN + SINAMICS G120. TIA Portal v15.1.
AttachmentProfinet_servo.zip (556 Downloads) |
Last edited by: Jen_Moderator at: 12/03/2021 09:19:13Removed link and added file as an attachment. |
|
12/3/2021 5:34 PM | |
Joined: 8/2/2019 Last visit: 1/12/2022 Posts: 12 Rating: (0) |
AttachmentTrace01.zip (659 Downloads) |
12/6/2021 1:49 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, something is wrong with your configuration. Try to move with drive control pannel, and compare values between TO and drive. Actual velocity and speed on drive side and position change depending on velocity. May be encoder configuration or referencevalues are wrong. Here is an example project: https://support.industry.siemens.com/cs/de/en/view/81666970 |
With best regards, |
|
12/6/2021 7:39 PM | |
Joined: 8/2/2019 Last visit: 1/12/2022 Posts: 12 Rating: (0) |
This is my config: [snip] Attachmentmy_project.zip (598 Downloads) |
Last edited by: Jen_Moderator at: 12/07/2021 08:08:32Removed link and added file as an attachment. |
|
12/9/2021 5:10 AM | |
Joined: 8/2/2019 Last visit: 1/12/2022 Posts: 12 Rating: (0) |
Do you mean to set parameters p1120/1121=0? |
Follow us on