12/11/2021 5:33 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877) |
Hello, CUA 32 adopter is used with DC/AC blocksize power module. Sinamics drive which you mentioned is 6SL3310-1TE32-1AA3 AC/AC converter power module which can be connected to CU320-2 via Drive CLiQ. Also in attached on line snap, no connection of CUA32 is shown. |
This contribution was helpful to1 thankful Users |
12/13/2021 9:31 AM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Dear Almen123, the CUA32 is used to connect an AC/AC power modules in blocksize format to a CU320-2 control unit. But as you can see on the following link the 6SL3310-1TE32-1AA3is a chassis format, which comes with Drive-Cliq interfaces. https://support.industry.siemens.com/cs/ww/en/pv/6SL3310-1TE32-1AA3/pi?dl=de As PISCEAN 2010 already mentioned, you can see in your topology screenshot that the Drive-Cliq of the 6SL3310-1TE32-1AA3 is directly connected the control unit Drive-Cliq port. So, no need for an additional CUA32. |
With best regards, |
|
This contribution was helpful to2 thankful Users |
Follow us on