1/15/2022 12:38 AM | |
Joined: 9/27/2006 Last visit: 5/6/2024 Posts: 12257 Rating: (2666)
|
Hello; To help you out, we would need more information on the Profibus/As-i gatteway you are woring with. The screenshot below is from the Bihl + Wiedeman website and shows the presently active models for their Profibus/As-i gateways. Searching for your gsd name on their site produces no results. The gsd_db website identifies the gateway as a 1568 model, with a xxxx1745 gsd file. Does that model number mean anything to you? You could try to download the file from the gsd_db website, but I have had no results recently, it might be inactive. http://www.gsd-db.net/view.php?gsd=15681745.gsd If that is the case, the Bihl+Wiedeman website states the the legacy gateway model 1568 gsd file is named 1568_gsd. Gsd file names can change sometimes over the years,Dowload it and examine the header of the file, it describes the unit is designed for, validate that it will work for your project https://www.bihl-wiedemann.de/us/products/index-archiv/archiv-mastergateways/t/bwu1568.html Daniel Chartier |
Last edited by: dchartier at: 01/15/2022 00:42:16 |
|
1/17/2022 4:03 PM | |
Joined: 4/28/2015 Last visit: 5/1/2024 Posts: 4 Rating: (0) |
Hi, Daniel. I try attach photo of my device: AS-Interface/ProfiBus Gateway 2.1 2-Master graphic display. 15681745.gsd, 1568.gsd, 15691745.gsd from gsd-db.net are not work. I have only upload from PLC. In Hardware Configuration this device write - need15001745.gsd. This is very old machive by Krones. |
1/17/2022 4:04 PM | |
Joined: 4/28/2015 Last visit: 5/1/2024 Posts: 4 Rating: (0) |
|
1/17/2022 4:17 PM | |
Joined: 4/28/2015 Last visit: 5/1/2024 Posts: 4 Rating: (0) |
ScreenShot from Hardware Configuration |
1/17/2022 4:53 PM | |
Joined: 9/27/2006 Last visit: 5/6/2024 Posts: 12257 Rating: (2666)
|
Hello; I have looked through the web and the Bihl + Wiedemenn site with no results for a 15001745.gsd file. There are 2 ways you could locate this file: 1. if you have access to the original PC the step 7 program was designed with, the gsdfile should be found in the project directory "<Drive:>\ ProgramFiles\Siemens\Step7\S7DATA\GSD". You couuld then copy it and integrte it in your new Step 7 project. 2. If nothing else works, contact Bihl + Wiedemann support and request their files for the BW 1500 As-i 2-master to Profibus model. Somewhere in their files they must have an archive that could help you. The cntact links to B+W support are shown in the screenshot below. You can also open the ontacts link, there you will find a Contact Form that you can use to send them a message, something similar to siemens Support request. Their techs should reply directly when they have the information you need. Here is my link to BIHL + Wiedemann site, since I am from Canada. You should try to find the one that matches your country of origin. https://www.bihl-wiedemann.de/ca/contact/canada.html Hope this helps, Daniel Chartier |
Follow us on