1/15/2022 5:35 PM | |
Joined: 2/8/2015 Last visit: 3/23/2024 Posts: 461 Rating: (8) |
Can every body help me, please? |
1/17/2022 7:14 PM | |
Joined: 2/8/2015 Last visit: 3/23/2024 Posts: 461 Rating: (8) |
Any solution please? |
1/17/2022 9:54 PM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello Tekabi; You are testing your redundant I/O program with PLCSIM? You might find this dscussion very interesting, pay special attention to Phantom_75's last post, where it is stated that: "you cannot test I/O redundancy using PLCSIM. The reason for this is, some of the system function blockscannot be processed "normally" by PLCSIM. See the following FAQ: What is the difference between S7-PLCSIM and a "real" automation system?" You misght have to wait until you hace actual hardware to do the FC 450 tests. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/17/2022 21:56:15 |
|
1/24/2022 8:51 AM | |
Joined: 1/11/2019 Last visit: 3/26/2024 Posts: 682 Rating: (138) |
Hi, No need add them manually, Chart folder download is sufficient for system generated charts and blocks. |
Follow us on