3/18/2009 1:41 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear sulung, Please have a look at this link: http://support.automation.siemens.com/WW/view/en/213253 Best regards, Wizard |
3/19/2009 8:59 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Yes this files are from old version of Protool. (All files are in a subirectory with the same name as the main file.) My opinion is you can't open with version 6.0. On the other side, this type of panel OP17 can be manage with Protool from version 3.0. Did you look at Wizard's link? About Prosave backup. You can only download to the same type of panel. Can't be editable this file. You want to migrate to WinCC Flex. In his case you need to change type of panel. Op17 is not supported by WinCC Flex. Look at WinCC flexible 2008 Migration (Migration from OP17 to OP177B). I suggest you to start to build by yourselves in WinCC Flex new project with new panel, using information from OP17 which you can see from prosave file backup.
You need tool to see this data. Look for in Google. I am sure, you can find it easy. regards |
3/20/2009 2:23 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello guys, I am sorry, my german is not so good. (english also). So, easier way is to try to find this alone in Google, but... well, look at decoder tool (http://rapidshare.com/files/169508189/DecoderProSave.exe). Output information is:
***Support: TD17,OP7,OP17,C7-633,C7-634 backup prosave file. regards |
This contribution was helpful to1 thankful Users |
3/23/2009 4:09 AM | |
Joined: 5/26/2007 Last visit: 4/26/2024 Posts: 127 Rating: (3) |
Dear UMENCHO, You are my angle. thank you very much. |
1/22/2022 10:36 AM | |
Joined: 11/7/2020 Last visit: 1/27/2022 Posts: 1 Rating: (0) |
UMENCHO, can u send me decoderprosave.exe link again?..it is a big help.. i need it immediately |
Follow us on