6/15/2006 2:30 PM | |
Posts: 14 Rating: (1) |
Hi everybody, |
6/17/2006 7:43 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315) |
[quote user="Maky7722217"] ihave to make Drive ES v5.1 SP3 runs on Windows 2003 Server. How can I do this? Any idea,pls? So far as I can see it is not tested, look in the pdfI have attached [:cry:] What do you want to do with Drive ES on the Windows 2003 Server ? Also V5.3 is now actual, maybe that that one works on a Windows 2003 Server, it is not tested, I don't know if it hen also not works... [:blush:] Attachments7komp_b.pdf (819 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on