7/9/2009 6:53 AM | |
Joined: 8/25/2006 Last visit: 4/25/2024 Posts: 2203 Rating: (277) |
1. Without archive you can go online only with IBS501. 2. It is not possible to upload program from FM458. |
7/9/2009 7:03 AM | |
Joined: 6/1/2009 Last visit: 1/4/2023 Posts: 27 Rating: (0) |
Hi KSN Can i online with XP OS. |
S.H.O |
|
7/9/2009 7:12 AM | |
Joined: 8/25/2006 Last visit: 4/25/2024 Posts: 2203 Rating: (277) |
XP OS is from NT family, so IBS works on XP, but you should test how it will work with FM. |
7/9/2009 1:43 PM | |
Joined: 8/31/2005 Last visit: 3/7/2024 Posts: 2197 Rating: (326)
|
The IBS501 is not released to be used under Windows NT (or higher), nor with the FM458. |
Last edited by: miami at: 7/9/2009 1:43 PM |
|
Follow us on