Industry Online Support
Technical Forum
11/10/2009 1:11 PM | |
Posts: 133 Rating: (2) |
Hi all. I wanted to know if I delete blockes (FB, FC, etc) in project window will it delete the same in flash memory card as well? thank you. |
11/10/2009 2:14 PM | |
Posts: 510 Rating: (117) |
The procedure for deleting the files on the MMCis contained in this FAQ, http://support.automation.siemens.com/WW/view/en/13992345 You have to open the online blocks to delete the MMC.If you have a PROM programmer you can insert the MMC and use the SIMATIC Manager > File > S7 Memory Card > Delete function as well. Regards, billwest |
11/10/2009 4:43 PM | |
Posts: 261 Rating: (42) |
Dear kanan, One note: Don’t format the MMC with any third party device to delete the program. Then it will be no longer ready to use. LINK regards ddg |
Last edited by: ddg at: 11/10/2009 10:10 PM |
|
11/15/2009 7:24 PM | |
Posts: 133 Rating: (2) |
Thank you guys! Answers was very helpful! Best regards |
Follow us on