11/11/2011 10:25 AM | |
Joined: 10/26/2005 Last visit: 9/13/2024 Posts: 284 Rating: (50) |
Hello, As I understand, you are using WinCC-Scada, then, please,use gsmgfuntion. Search this forum, and find example! From online support, FAQ: At Runtime, how can you determine the message texts or process-associated values when a message appears in the associated, user-specific action "GMsgFunction()"? http://support.automation.siemens.com/WW/view/en/25678075 To use SQL in C, create a command-file and execute it! An example of SQL in C-skript in WinCC, using "programexecute" http://support.automation.siemens.com/WW/view/de/23370769 |
Last edited by: perdahlqvist at: 11/11/2011 10:32 AMLink to gsmgfunct.. |
|
This contribution was helpful to1 thankful Users |
11/11/2011 11:18 AM | |
Posts: 12 Rating: (0) |
Dear perdahlqvist.
Thank you for your help, regarding GMsgFunction, I’ll check it out. But, the SQL part is a problem, because on the link you’ve sent, it says that it only works until WinCC V5 SP1 |
11/11/2011 12:53 PM | |
Joined: 10/26/2005 Last visit: 9/13/2024 Posts: 284 Rating: (50) |
Hello! Yes, the SQLsyntax part is not valid(wrong WinCC version). The C-scriptwith SQL is the important stuff... |
11/22/2011 10:30 AM | |
Posts: 12 Rating: (0) |
I'm doing some work arround this issue. I'm studing the GMsgFunction, to get what I need from the messages, at the moment, I get almost every thing I need, but with a lot of C-Script code. Regarding the SQL, I'm using a comand line program from SQL Management: sqlcmd |
Follow us on